This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AHC1G14: Logic forum

Part Number: SN74AHC1G14


Hello team,

I am shweta chendake From knorr -bremse technology center india

i working on SN74AHC1G14DBVR IBIS model in that input  models were not working properly

according to an IBIS specification  The voltage column in the [POWER Clamp] should extend at least from -Vcc to 0 (it is permitted
and recommended to extend from –Vcc to +2 * Vcc

i am trying to drive this input pin with 7V means the ESD protection diode should able to drive upto 5V only but this is not working