This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV2T74-Q1: Static power when the output Q is low

Part Number: SN74LV2T74-Q1


Tool/software:

Hi team,

My customer is concerned about the static power of SN74LV2T74-Q1 under the following condition:

Only one channel is used. Vcc=5V, D, nPRE and nCLR are pulled up, CLK is low, nQ is floating.

In my opinion, the max static input current is 20uA. Is that right?

Best Regards

Grey