Tool/software:
Hi TI
SN74LVC2T45QDCURQ1 output short to gnd,I use a resistance limit current. does 50mA is enough?
Such as below show Vccb is 5V,B2 short to gnd,and the limit current is 50mA,does damage the IC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi TI
SN74LVC2T45QDCURQ1 output short to gnd,I use a resistance limit current. does 50mA is enough?
Such as below show Vccb is 5V,B2 short to gnd,and the limit current is 50mA,does damage the IC?
Thanks for your reply
beacuse of output has parasitic capacitance(~300pF),output PWM frequency is 800KHz.
if the resistance is too large,will increase output rise time.
Hello Ling,
Like Clemens said, this should be fine but 50mA is the limit. I would recommend slightly increasing the resistor to maybe 110 Ω so we are not at the 50mA limit.
Regards,
Josh