Using a SN74LCVH244A and have a question pertaining to the input current. Ii on the datasheet states +-5uA max. If the input is either going to be a GND or a pull up to 3.3V, does this imply that the pull up resistor is very large, given that the input current is very small?
R = 3.3V / (5 x 10^-6A) = 660K resistor. Does this seem correct?