Part Number: SN74ABT541B
Tool/software:
Team, I'd like to confirm if this device has only low side clamp diode as VI<0, IIK=-18mA and High side has no clamp diode on the input pin? thanks.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74ABT541B
Tool/software:
Team, I'd like to confirm if this device has only low side clamp diode as VI<0, IIK=-18mA and High side has no clamp diode on the input pin? thanks.

One more question, when VCC = 0V, and Input voltage is 3V or 5V. With this condition, does device work normally? Or is it risky?
Yes, ABT input are overvoltage tolerant. See [FAQ] Can the input voltage (Vi) to my logic device be higher than the supply voltage (Vcc)?
When VCC = 0 V, larger input voltages are allowed by the absolute maximum ratings. No current will flow, and the device will not power up.