Other Parts Discussed in Thread: SN74LVC3G14, SN74LVC1G14, SN74AC14
Tool/software:
Hi team,
Looking at the data sheet for the SN74LVC14APWR, the recommended operating voltage range is 2V to 3.6V, suggesting that it is intended for use at a 3.3V level. Looking at the electrical specifications table, it is written that it is specified for up to 3.6V, so I believe it is intended for use up to 3.3VI/O
On the other hand, the maximum rating is 6.5V, and the output voltage is Vcc+0.5V, so it appears that the device can also operate with a 5V interface. If the power supply voltage is 5V, can I refer to the 3.6V specifications? Or is it possible to operate with a power supply voltage of 5V, but not guaranteed?
The SN74LVC1G14DRLR, a single-gate type with the same logic, has a recommended voltage range of 1.65V to 5.5V, and it is clearly stated that it is OK to use it at 5VI/O. Could you please tell me the differences between SN74LVC14APWR and SN74LVC1G14DRLR (single-gate type)?
Thank you for your help
Regards,
Taito Takemura
SN74LVC14A datasheet (Absolute maximum and Recommended conditions)