This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G07: SN74LVC1G07DCKR

Part Number: SN74LVC1G07

Tool/software:

Hello team,

i am validating an IBIS model of  below  part which is Open drain type

SN74LVC1G07DCKR

 

i am getting warning ftom IBIS parser test that is - Model 'LVC1G07_OUT_33': MAX VI curves cannot drive through Vmeas=1.5V
given load Rref=500 Ohms to Vref=0V

According to IBIS Quality specification For Open-drain models [Model] or [Model Spec] Vref must be above Vmeas, and it is usually set to the [Pullup Reference] voltage.

But in IBIS model file of given model Vref is 0 

can you please explain the reason behind this or any quality report of this model is there ?

regards,

shweta