Tool/software:
Hello Team,
I need an information regarding the reflow profile of components with Ni Au Pd plating.
I have to produce PCBA in SnPb process with peak max at 220°C. In my opinion, the RoHS process with peak max at 245°C will be more adapted in case of NiAuPd finishing. I'm not sure that the intermetallics will be sufficient with SnPb process. I’d just need a confirmation > Is the Ni Au Pd plating is compatible with Sn Pb profile ?
Thank you for your help.
Regards,
Renan