This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS02612: SDIO waveform issue on CLKB1 pin

Part Number: TXS02612

Tool/software:

Hi all,

I have designed a system in where SDIO signals for uSD-CARD need to be shifted from 1V8 to 3V3 in DS mode (25MHz) or HS mode (50MHz).

From debbugging, we found a problem on the waveforms.

This is part of my schematic:

This is the waveform at 25MHZ (SDIO0_SDCLK in RED and SDIO0_SDCLK_CARD in YELLOW)::

 As can be seen, there is some sort of overshoot between 1.5 and 2 V on the output signal at 3.3 V (yellow).

The same at 50MHz:

And at 195KHz:

The SDIO BUS signal traces are made with an impedance of 50Ohm and the same length.

Do you have any advice to explain this behavior?

(Teledyne ZS1500 and HFP1500 active probes were used for these measurements.)

thank you in advance for the support.

Best regards.

Stefano Asiri.