Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC4T774: SN74AVC4T774PWR max cap load

Part Number: SN74AVC4T774

Tool/software:

We want to know max drive capacitive load capability for level shifter.

Can anyone help provide max capacitive load capability ? thanks

  • The datasheet's test condition is 15 pF. You can use higher capacitive loads up to about 70 pF. For even higher loads, your circuit must ensure that the (dis)charge current does not exceed the absolute maximum rating of 50 mA.