Part Number: TXS0104E
Other Parts Discussed in Thread: TXS0101, TXS0102, TXS-EVM
Tool/software:
Hello,
Is there a SPICE model or equivalent I could use for this device?
Background info: I have this device on a signal that is shared between two PCB boards. I am trying to model what happens when one board loses power and the other one does not. This signal goes from an MPSOC on one board to the TXS104E device to another MPSOC on the other board. We believe the MPSOCs internal ESD diodes on the power loss board are unintentionally pulling this signal low on both boards. Given that this device also had ESD diodes as evidence that the max output voltage rating on the datasheet shows Vcc+0.5V, I wonder if the same issue with occur? I am also wondering how the one-shot function will behave for this device if one board goes low and the other does not.
If no equivalent spice model exists, could you help explain how I can best model this device?