This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HCS153-Q1: Requesting failure rate

Part Number: SN74HCS153-Q1


Tool/software:

Hi, 

Can I get the failure rate (FIT) for this device (SN74HCS153QPWRQ1)? 

I am using the Motor Control mission profile based on IEC 62380 (Table 11 - Mission profiles for automotive). Mean temp ~60 deg C.

Preferred confidence levels of at-least 70%. Happy to help with any additional information needed.

Regards,