Other Parts Discussed in Thread: TXV0108
Tool/software:
Hello.
As written in the title, I would like to request a review because it appears to be an error in the data sheet. (descriptions that has a fixed direction but is treated as bidirectional.)
page 1 - RGMII Applications; The above block receives input from VCCA and outputs from VCCB. It receives input from VCCB and outputs from VCCA.
page 3 - Pin Functions; A1~A6 should be for input only, and B6~B1 should be for output only, but both are for both input and output.
page 20 - Using the TXV0106 for Power Isolation; Same as page1.
Since it was being used in two ways on page 1 & 3, I briefly reviewed it and designed it as a bi-directional product, but a big problem arose during debugging.
Please review the typical application and pin descriptions on the first page one more time to ensure they are entered accurately.
In addition, it would be nice if the bi-directional product line also had this size 3.5 x 2.5 mm and A1 & A2 are placed consecutively.
Thank you for reading.
S.Y.Lee