Other Parts Discussed in Thread: SN74LVT16245A
I have a 75LVT1624 part in my design that ha s the bus-hold feature in the part, so data sheet says resistors for pull-up or pull down are not recommended. If one does put a 10K pull-up or 1K pull down does it harm the part or effect it’s long term relaibility?
The pull ups/downs are on the inputs, but since the part is bi-directional, they can become outputs.
During power-up does the part end up in deterministic state on the I/O because of the buss-hold feature or is the state random?
Thanks and Best Regards,,
-Tim Starr on behalf of MG@DE