TXB0104: Question about the application of SPI signal

Part Number: TXB0104

Tool/software:

We would like to use two TXB0104RUTR as SPI signals buffer because the traces are too long.

My question is the datasheet mentions the "Maximum data rate" is 60 Mbps, does it need to div 4 to get 15Mhz for support single signal max frequency?

Note: Current our design is Quad SPI with 16.6Mhz and may up to 33.3Mhz or 66.6Mhz.