This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1T45: Can support translation of 0.65V to 1.2V at 100Mbps?

Genius 17425 points
Part Number: SN74LVC1T45
Other Parts Discussed in Thread: SN74AXC1T45

Tool/software:

Hi Experts,

We have queries about SN74LVC1T45DBVR.

Can it effectively translate from 0.65V to 1.2V at a 100Mbps data rate, as well as from 1.2V to 0.65V at the same data rate?

If not, do we have product that support this translation?

Regards,
Archie A.

  • Hi Archie,

    LVC is not recommended for 0.65 V. See SN74AXC1T45.

    Unfortunately, we do not have a 100 Mbps device for 0.65 V as of this time. Please follow-up offline via email as we can further discuss how to support customer for newer devices, thanks.

    Best Regards,

    Michael.