TIBPAL20L8-20M: Clarification RE MIL and orderable part numbers for PAL component

Part Number: TIBPAL20L8-20M

Tool/software:

TIBPAL20L8-20MJTB seems to be a currently orderable P/N (24 pin CDIP package).

Can TI supply this part under any of the following standards:

5962-8767101LX

JM38510/50501BLX

8412901LX

This would simplify our approval process to support an old design (this is the same product as referenced in the linked thread).

  • In reference to the linked thread, there was a question about a 30 ns spec.  This refers to the Prop-delay differences that exist between the original (circa 1990) MIL specs (5962, JM38510, and 84129).  We need to at least meet the worst-case spec for each of the three MIL P/Ns referenced in my OP.

  • Hi Joseph,

    From what I can tell given the device marking, the part should follow the 5962 standard.

    Best,

    Malcolm