Part Number: LSF0002
Tool/software:
Hi,
Does TI have a 2-bit bidirectional buffer (push-pull) solution? <= Do not suggest the TXB series because it requires over 100Kohm pull-up resistors and cannot be used.
The speed should support over 10Mbps.
By the way,
- For ICE TMS TCK signal
- 2-bit bidirectional buffer (Push-pull) solution with auto-detect direction
- Speed of at least 2-3Mbps, preferably over 10Mbps
- Signal needs to be reinforced due to long cable length, signal regeneration (repeater) would be preferable
Thanks!
Jeff