Part Number: TXB0102
Other Parts Discussed in Thread: TXU0202
Tool/software:
I recently added TXB0102 to make the UART level translation from an MCU at +3.3 V (PIC18F47J13) to send AT Commands to a Modem at +1.8 V (Quectel BG600L-M3), however, in my design I have the MCU in the B side of the translator and the Modem in the A. Could this cause any issues?
As well, the OE and VCCB are coming together from a GPIO of the MCU while VCCA is coming from a +1.8V pin from the modem itself.