This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G04: Inverter that supports level conversion with VCC=5V, Vin=3.3V, Vout=5V output

Guru 12115 points
Part Number: SN74LVC2G04
Other Parts Discussed in Thread: SN7404, SN74AHCT1G04, SN74LV1T04

Tool/software:

Hi,

I am looking for an inverter IC that supports level conversion with VCC=5V, Vin=3.3V, Vout=5V output. The specs are similar to TC7PZ04FU, and pin-compatible with SOT-363 would be helpful.

Looking at the cross reference, SN74LVC2G04DCKR is recommended. However, with SN74LVC2G04DCKR, when VCC=5V, VIH≧3.5V, which exceeds the 3.3V input.

Are there any solutions you can suggest?

Thanks,

Conor