This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV123A: Upper and lower limit for pulse width

Part Number: SN74LV123A

Tool/software:

Hi experts,

The output pulse width t_w is determined by the following equation:

t_w = K × R_T × C_T

Is there an upper and lower limit for pulse width t_w that can be set?
(For example, is it OK to set t_w=60s?)

In addition, are there upper and lower limits for resistor R_T and capacitor capacitance C_T in this device? As for the upper limit, I thought that if there were no problems with the size of the capacitors and resistors, the pulse width could be as large as possible, but what about that?