This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74VMEH22501: Need clarification on electrical parameters of SN74VMEH22501

Part Number: SN74VMEH22501

Tool/software:

Hi Everyone,

I need some clarification on below highlighted:

1. What should be voltage level at pin 42 and pin 31? what is the application of pin42 and pin31?

2. Why we used 1.5V in below image?

3. What is EEF Rtt represent in circuit? is it pull-up resistance?

4. GTPL is compatible with VME Backplane logic or not?

5. Is there any isolation between 3A and 3B port?

Let me know if you have any questions.

Thanks,

Gaurav