Part Number: LSF0108
Tool/software:
Hi!
I'm not sure this is the correct place to ask this, but I'll go ahead anyways.
In the LSF0108 data sheet reference schematics, it is recommended to place a 200KOhm resistor and a 1uF capacitor on the EN input. Sometimes, however the 1uF is replaced with a 1mF capacitor, which seems like a mistake to me.
The 1 uF value is specifically recommended in the '9.2.1.1.2 Bias Circuitry' section of the data sheet, while the 1mF value is only seen in figure 9-5 'Single Supply Translation with 3.3 V Supply'.
Could someone confirm this if this is indeed correct, or a mistake in documentation?
Thanks!