Part Number: SN74GTL2003
Other Parts Discussed in Thread: LSF0108
Tool/software:
Hi Team
My customer would like to consult with you and discuss the internal MOS action principle of SN74GTL2003. The picture below is the internal circuit of SN74GTL2003. From the picture, it shows the current wiring method and action. However, the customer is very curious that from the action point of view, N-MOS VGS If it is turned on, VDS will also be turned on. Logically speaking, D1 will also be 1.8V. Why is the potential of D1 3.3V?

Thanks,
Boyan