This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUP1G07: HBM and CDM pretection check

Part Number: SN74AUP1G07


Tool/software:

Hi 

Can you help to check.

De we meet this condtion, thank you.

HBM: ANSI/ESDA/JEDEC JS-001 class 3A exceeds 5000 V

• CDM: ANSI/ESDA/JEDEC JS-002 class C3 exceeds 1000 V