Part Number: SN74LVC1G123
Tool/software:
I need a circuit that when input goes high (5V) the output will go high for approximately 180 seconds. (The tolerance can be +/-20 %)
Will the SN74LVCG123DCUR work for this application.
The size of the capacitor and resistor would need to be very large in order to get such a long period.
But these size components are not within the range of component values specified in the datasheet
Is there better part choice for this application?
Note: the output is driving a fire extinguisher, so it cannot turn on when powered up like some of the one shots TI has.