This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G17: Can I use this device to convert from 3.3V to 5V as a logic level translator?

Part Number: SN74LVC2G17
Other Parts Discussed in Thread: SN74LVC2G14, UCC37324, SN74HCT14

Tool/software:

Hi,

 I want to use the SN74LVC2G17DBVR to do a logic-level translation from 0-3.3V signals on the inputs and convert them to 0-5V signals on the outputs. Can this device do this reliably? The supply voltage is 5V. If not can you recommend a part that can do this reliably? The output current needs to be at least 30mA per output. Please let me know at your earliest.

Thanks,

Eric Norton