Other Parts Discussed in Thread: TXV0108-Q1, LSF0108-Q1, LSF0108, TXS0108E
Tool/software:
Hi Team,
In our design, we are going to use TXS0108E-Q1 IC for MII Mode (Speed: 100Mbps) interface (TX and RX pin connection are connecting in only one Level translator). Can we use this level translator for MII Mode?
Please suggest other level translator for MII mode interface, If it is not suitable for MII Mode.
Specification :
- Voltage is 3.3 V to 1.8V and 1.8V to 3.3V
- 10Mbps data rate
- Bi-direction.
Regards,
Virali