This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0101: Request for proposals for alternatives that do not have internal pull-ups

Part Number: TXS0101
Other Parts Discussed in Thread: TXU0101, 2N7001T, SN74AUP1T34

Tool/software:

Is there an equivalent device that does not have an internal pull-up?
Unidirectional is fine, not bidirectional.

The background of my inquiry is as follows,
We want to shift the UART signal voltage from 1.8V to 3.3V at 115.2kHz.
We verified the operation of the TXS0101DCKR, which has a proven track record in our company, but the system stopped working.
After isolating the cause of the problem, it was found that the problem was caused by an internal pull-up.
We are looking for a device that does not have an internal pull-up.

I have previously had TXU0101, 2N7001T suggested as an alternative, are there any other products that could be considered as an alternative?