Other Parts Discussed in Thread: CD14538B
I am trying to replace a 74C221, as it is obsolete, with the CD14538B. The data sheet states wide range of output pulse widths. What is this range? I would like one of the circuits to have a 2.2uS period and the other to have a 30uS period. For the 30uS period the equation T= 0.5 RC gives R = 5K Ohms and C = 12nF. Because C is greater than 5nF do I use the equation T = RC. This yields C = 12nF and R = 2500 ohms which is below the 4K minimum. So if I half C to 6nF this equation yields C = 6nF and R = 5K Ohms. So should I use C = 6nF and R = 5K Ohms to achieve my 30uS pulse? As for the 2.2uS period the equation T = 0.5RC gives R = 4K and C = 1.1nF this falls in the acceptable values for C to use this equation. So should I use R = 4K and C = 1.1nF for my 2.2uS pulse? I had other questions about the part but DigiKey was able to provide those answers.