Tool/software:
Dear Texas Instruments Team,
I am currently performing power dissipation calculations for the inverting buffer amplifier PN: SN73LVC1G14QDCKRQ1. In the LVC characterization document, I found two different formulas for power dissipation—one for rail-to-rail inputs and another for TTL level inputs. However, the datasheet for the SN73LVC1G14QDCKRQ1 does not specify which input type the inverting buffer uses.
I would appreciate it if you could confirm whether it is appropriate to use the formula from the LVC characterization document for this purpose. If so, please clarify which of the two formulas—rail-to-rail or TTL level input—applies to the SN73LVC1G14QDCKRQ1.
For your reference, here is the link to the document I am referring to: LVC CHARACTERIZATION INFORMATION
Additionally, the formula includes an internal parasitic capacitance term, which is calculated using dynamic current. Could you please confirm if this dynamic current is the same as the peak current?
Lastly, we are using this buffer between two microcontrollers with a 5V PWM signal input. Will this setup lower the output voltage?
Thanks & Regards
Lithesh