Other Parts Discussed in Thread: TXV0108
Tool/software:
Dear TI,
We would like to understand whether SN74AVC32T245 can meet the switching characteristics of THC63LVD1024 or not while converting 3.3V logic to 1.8V logic.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Dear TI,
We would like to understand whether SN74AVC32T245 can meet the switching characteristics of THC63LVD1024 or not while converting 3.3V logic to 1.8V logic.
Thanks
The propagation delay is specified as 3.8 ns, which corresponds to at least 263 Mbps = 131 MHz.
Hi Uday,
200 Mbps = 100 MHz.
Furthermore, TXV cansupports 500 Mbps at 25 C and 420 Mbps 1.8V to 2.5 V and 400 Mbps 2.5 V to 1.8 V, thanks.
Best Regards,
Michael.
Hi Michael,
Thanks for the info. We are looking for 3.3V to 1.8V translation. What are the parameters that are to be looked at while selecting the device?
Hi Uday,
Per your system requirements, you may confirm operating voltages, I/O voltages, input data rate rate spec, propagation delay, output loading, interface type and any other special requirements such as partial-power down etc, thanks.
Best Regards,
Michael.
Hi Michael,
We want to level shift 3.3V logic IOs of THC63LVD1024 to 1.8V to interface FPGA
Hi Uday,
I do not see any issue as the above suggestions work well.
To double confirm, what is the data rate frequency of the signal sent from THC to FPGA? And any other FPGA requirements of concern missing in the level-shifter data sheet?
Best Regards,
Michael.
The max data rate which we require is 135MHz. The translation is from 3.3V to 1.8V.
No other specific requirements from FPGA side.