Tool/software:
Hello,
I would like to have 8 sensors connected to 1 spi bus. ssi0rx,ssi0tx,ssi0clk are connected as a bus wide manner.
However for the CS lines of the spi slaves, instead of using GPIO, i would like to use CD74AC138 or better part. the address lines are to be connected to gpio, The Y0 to Y7 are to be connected to the spi slaves, and the spi0fss is connected to _G2A or _G2B.
So basically I need a 3-line to 8-line decoder with negated outputs.
Any ideas or a better chip to do this task?
Best Regads,
C