Part Number: TXS02326A
Tool/software:
I want to run these two chips in parallel with 1 modem so I can utilize 4 outputs. Is there an EN function so that I can disable one of the IC's when I am multiplexing?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Cho,
The OE function of this device is to control the direction of data direction between UICC and SIMDATA and will not be able to enable/disable the device. You may need to drive EN1 and EN2 low together to disable the power supply of SIM1 and SIM2, as well as the interface itself.
Regards,
Jack