Other Parts Discussed in Thread: SN74ABT541B
Tool/software:
1. What's the topology difference between SN74ABT541 and SN74LV541?
2. Is the output of the SN74LV541AT able to connect to pull-high 5V rail? It looks the abs rating is different for both devices for VO?
SN74LV541AT => VCC+0.5V; When VCC=0V, the VO derating is only 0.5V~
SN74ABT541B=> 5.5V
Regards
Brian