This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G17: SN74LVC1G17DCKR Input current specification

Part Number: SN74LVC1G17

Tool/software:

Hi,

I want to ask about the input current for SN74LVC1G17DCKR.

It is written in the datasheet that the input current, A, needs to be a maximum of 5µ A. However, I have trouble finding any reference design that actually mention that we need to control the input current and explaining why.

I am supplying 3.3 V through an optocoupler into the Schmitt Trigger and to get 5µ A, I will need a series resistance of 660k Ohms and this will be slow down our IO response time a lot. I would like to know if it is okay to use about 68k Ohms (~50m A) instead of 660k Ohms?

Appreciate any help I can get. Thank you.