This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0102: Schematics Review

Part Number: TXS0102

Tool/software:

Hi  

I would like to  convert I2C signals logic levels 

Case 1) From logic 3.3V to 2.5V & I2C signals from MCU.

 

Case 2) From logic 1.8V to  2.5V & I2C signal from FPGA (Pull ups added near FPGA side) Via Board to Board Connector and then connected to TXS part input.

 

Kindly review the above schematics and please let me know any changes required. 

Additionally can we use the TXS0102DQER part for GPIO (Reset ) Level Translation from 3.3V to 2.5V?