Part Number: LSF0108
Other Parts Discussed in Thread: BQ4050, TCA9801
Tool/software:
I connected between SMARC module (IMX8 anao) and several i2c periferals the levelshifter LSF0108 to confert 1.8V to 3.3V:

There is 470k pullup on the IMX8 1.8V side (internal pullup).
If I put 10k pullup on 3.3V side, the signal is very bad:

And if I change pullup from 10k to 2.2k the signal seams better but the BQ4050 doesn't work...

Why the signal is very bad with 10k pullup ?
Is there too many devices on the bus ?
What is the best way to use the LSF0108 ?