Part Number: SN74ACT244
Other Parts Discussed in Thread: SN74LVC2G07, SN74LXC8T245, TPL7407LA, TPS22996, TPS22960, TXU0104, SN74LXC2T45, CSD13381F4
Tool/software:
Hello,
I have 8 LED and each LED can have a forward current of 25mA with forward voltage as 1.7V.
I want to turn on or off each LED independently using Microcontroller IO where IO follows 1.8V logic level (i.e. High = 1.8V and Low = 0V)
The LED can be powered using 3.3V source.
Is there a non-inverting buffer which I can use for such purpose?
Regards,