Part Number: TXU0104
Tool/software:
The TXU0104 datasheet indicates that if one of the supplies is disconnected or is below 0.1V, the outputs are set to a high-impedance state. In this case, how much current is drawn from the supply that IS connected? The specific case I'm interested in is when VCCA = 3.3V, VCCB is disconnected, and the inputs (on the A side) are being driven. In this case what current would be drawn from VCCA (approximately)?