This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AXC4T245: level shifter chip suggestion needed

Part Number: SN74AXC4T245
Other Parts Discussed in Thread: SN74AVC16T245

Tool/software:

I want to connect my CC3230SF12RGKR MCU (3.3V GPIO) to my Cellular + GNSS modem (1.8V GPIO) via a single-level shifter. The cellular modem talks to the MCU via UART (8 lines). Two additional lines are required for GNSS NMEA, TX, and RX. Is there any cost-effective single-level shifter chip that can do the task? I want a single-level shifter that can translate for 10 GPIOs.