Other Parts Discussed in Thread: TXV0108
Tool/software:
Hi, I wish to use the TXV0106 for power off buffering of an RGMII bus between a SOM and a ethernet switch. The ethernet switch can be powered down to save power if if it is not needed and the RGMII bus would be a source of back powering to the switch without the buffers in place.
I wish to know if the 10 Ohm damping resistors are on the inputs (A side) or the outputs (B side) or both and if I require external 32 Ohm series resistors on both the input and the output. So a resistor between the SOM output and the buffer and then another resistor between the buffer and the switch?
Thanks
PS. The TXV0106 datasheet is still has some errors copied and pasted from the TXV0108. Specifically the pinout in table 4-1.