Other Parts Discussed in Thread: TWL1200
Hi All.
We're considering the usage of the TWL1200 level shifter to connect a WiLink6.0 based WIFI+BT combo solution (with 1.8V I/O) to a host SoC that operates @ 3.3V levels.
WiLink6.0 requires a reference clock input, one of the WiLink6.0 supported reference clock options is a digital, 1.8V referenced 26MHz clock.
Our system can provide only a 3.3V referenced 26MHz digital clock. This means that we need to "down-shift" the 3.3V 26MHz clock to 1.8V voltage levels.
Since we intend to use TWL1200 level-shifter for SDIO and UART translation, and we do not plan to use the AUDIO interface of WiLink6.0, the AUDIO part of TWL1200 remains unused.
What I've had in mind is to use the AUDIO_CLK translation terminals of TWL1200 for our 3.3V 26MHz clock translation to 1.8V, My question is whether this is possible? I could not find maximum data rates for the AUDIO section of TWL1200 in the TWL1200 datasheet.
Thanks.
Alex M.