Other Parts Discussed in Thread: SN74LVC1T45
Hello,
I am studying the SN74LVC1T45 to check if this component can be the best choice in a new product, and I am quite confused about the information I read in the datasheet. For example if I use this buffer to operate both input and output ports to 3.3V, I understand that the max data rates is 210 Mbps, which normally corresponds to a minimum bit duration of 4,76 ns.
Now the switching characteristics give a maximum tplh to 5.8 ns and tphl to 5 ns. Both values normally define the tpd of the buffer. So how can I get a max data rate of 210 Mbps if the tpd is defined to max 5.8 ns?
By the way, on Texas Instrument internet page of the 74LVC1T45 (http://www.ti.com/product/sn74lvc1t45), Parametrics table indicates a max tpd of 3.9 ns, which I don't find in the component's datasheet. Is there another datasheet with this information?
Now how should I understand "max data rate" and "switching characteristics" ? I've read the application report "Understanding and Interpreting
Standard-Logic Data Sheets" (szza036b.pdf) but it did not really help me to clarify my mind.
Regarding my application, my main concern is to clearly control the propagation delay time of a synchronous bidirectional line which max data rate would be 50 Mbps.
Thank you for any help,
Regards,
David