Part Number: LSF0108
Other Parts Discussed in Thread: TXU0304
Tool/software:
Can LSF0108 be used for SPI level conversion?
If possible, is there a reference design for converting 1.8V SPI to 3.3V SPI interface using LSF0108?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
It might be possible, depending on the required speed and on the drive strength of the devices. A reference design does not make much sense because sizing the pull-up resistors depends on the characteristics of the actual board.
A buffered translator like the TXU0304 is much better suited for this application.