This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV6T17-EP: Need part number suggestion

Part Number: SN74LV6T17-EP
Other Parts Discussed in Thread: SN74HCS05, SN74LVC1G16, SN74LVC2G07, SN74LVC07A, SN74LVC2G17, SN74HCS365

Tool/software:

I am looking for dual and 6 channel buffer IC. 

below are specifications:

Dual channel :

1. Input type : Schmitt-Trigger

2. Output type : open Drain

3. Operating voltage : 5V 

4. Number buffers in one IC : 2 buffers 

6 channel :

1. Input type : Schmitt-Trigger

2. Output type : open Drain

3. Operating voltage : 5V 

4. Number buffers in one IC : 6 buffers 

Thanks and Regards

Shubham Bajpeyee

  • There is no such device.

    The combination of Schmitt-trigger inputs and open-drain outputs exists only for inverters, e.g., SN74LVC1G16, SN74HCS05.

    If you cannot change the polarity of the signals, then you have to combine a Schmitt-trigger buffer (e.g., SN74LVC2G17, SN74HCS365) with an open-drain buffer (e.g., SN74LVC2G07, SN74LVC07A).