Part Number: SN74LVC1G07
Other Parts Discussed in Thread: TXU0101, SN74LVC1G34
Tool/software:
What is the maximum frequency you can push through this device (SN74LVC1G07)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LVC1G07
Other Parts Discussed in Thread: TXU0101, SN74LVC1G34
Tool/software:
What is the maximum frequency you can push through this device (SN74LVC1G07)?
This device has an open-drain output, so the speed of rising edges is limited by the pull-up resistor and the load capacitance.
If you need a high output frequency, use a buffer with push/pull output like the SN74LVC1G34/17. For level shifting, use something like the TXU0101.
Thanks for you reply. Assuming load capacitance is non existing and having a pull up of 2.5k. What would be again the max frequency? I need an open drain/collector buffer
A CMOS input has a capacitance of < 10 pF; traces have a capacitance of roughly 1 pF/cm. R and C form a low-pass filter.