Other Parts Discussed in Thread: SN74LV8154, SN74LVC1G17, LMV7219, SN74LV4040A
Tool/software:
Hi TI Technical Support Team,
I am designing a PCB which will be used to count/measure the frequency. The measured frequency will be proportional to the concentration of the parameter. The frequency range can be between 1MHz and 50MHz. I am planning to use SN74LV8154 as 32 bit counter to count the edges of the signal. My input signal is noisy sine wave.
In my initial test setup, I used SN74LVC1G14DBVR as Schmitt Trigger to convert sine to square wave, such that I can count edges of the square wave to measure the frequency. I used 16MHz crystal oscillator as reference signal. The output of SN74LVC1G14DBVR is given below. I think when the frequency of the input sine wave will be near 50MHz, the waveform will be even worse. Could you please suggest me proper schmitt trigger IC (or maybe another method) so that I can convert sine wave (max frequency about 50MHz) to square wave?
Thank you for your help,
Ahmet