Part Number: SN74LVC16T245-EP
Tool/software:
Hi Sir,
I am using "CLVC16T245MDGGREP" from the "SN74LVC16T245-EP" family
I have activated enable and direction pins but am not giving any inputs to input pins (For Eg-1A1) it is in a high impedance state. Is it okay not to connect anything to these pins? what problems will I face if I do that?
In the datasheet, it was maintained that " All unused data inputs of the device must be held at VCCA or GND to ensure proper device operation."
I activated A data to B bus means the input will be A side and the output will be B side. Should I connect both the input and output side with GND/VCC? Do I need any pull-up/pull-down resistors?