Other Parts Discussed in Thread: TXU0104, SN74LXC8T245, SN74AHC541
Tool/software:
Hi all,
Planning to use a TXB0108 level shifter for converting 5 V to 3.3 V to interface with my Zynq 7000 FPGA. Schematic photos as attached.
The inputs are mainly I/O signals generated in TTL format which i have to convert to 3.3 V for use in my FPGA
Is there any other circuitry which is needed for this, or is this the right implementation.
Any resistors, capacitors etc
Also do we need isolators for removing noise for such inputs to FPGA?
I ask Because these inputs are being generated in a circuit which has high voltage components and there may be noise on the path from there to here.
The Connector on the right is the Mating Connector for the FPGA.